FactoryTalk Batch Server option configuration
Configure the
FactoryTalk Batch
Server and FactoryTalk Event Archiver
using the Server Options
dialog box in FactoryTalk Batch Equipment Editor
. The configuration information for the server indicates how it communicates with FactoryTalk Batch
clients and the data server(s). Configure FactoryTalk Event Archiver
to specify if and how electronic batch record files (.evt
or .evtj
) are
inserted into the ODBC-compliant database.Changing items such as
FactoryTalk Batch
Server information, area model, and the error logging directory take effect when the
server is restarted. Changing items such as the recipe directory and batch journal directory
take effect the next time the server accesses these items. None of the items in FactoryTalk Event Archiver
configuration require the server to be restarted. These changes take effect the next time
the server needs that configuration item.
IMPORTANT:
FactoryTalk Batch
does not support the use of mapped drives. Do not use mapped drives for project directories.Provide Feedback