Cross Invocation Descriptors and Defaults tab
The
Cross Invocation Descriptors and Defaults
tab allows you to specify cross invocation labels and set default cross invocation strings for different resource types. Use FactoryTalk Batch Equipment Editor
to define up to five cross invocation strings for each resource within the area model. Each time a selection changes in FactoryTalk Batch View
and HMI Controls, the cross invocation strings associated with the equipment resource are retrieved from the FactoryTalk Batch
Server and evaluated. The contents of these strings can indicate a shortcut menu item and subitems, the caption(s) for the shortcut menu item(s), and the data that is passed to the automation server.
Provide Feedback