Default values
Use the
Default Values
area to assign default URLs to each hyperlink label defined for the selected resource type. Enter the URL address for the hyperlink in the box that corresponds to the correct hyperlink label. The label in box 1
of the Descriptors
area corresponds to the URL address in box 1
of the Default Values
area. Default URLs can be overwritten when a specific resource type instance is edited.
TIP:
If a hyperlink value is not defined, either as a default or when the specific resource
type instance is created, the hyperlink label is not visible in .
e
ProcedureProvide Feedback