Hyperlink Descriptors and Defaults tab
This feature is used in conjunction with only.
FactoryTalk
e
ProcedureThe
Administrator Guide for additional hyperlink information.)
Hyperlink Descriptors and Defaults
tab specifies the hyperlink labels and
default values used with different resource types. The labels and default values are used in
the resource’s Edit
dialog box. You can define up to five hyperlink labels and
default values for each resource within the area model. (Refer to theFactoryTalk
e
ProcedureThe
Resource Types
list allows you to select a resource type for the hyperlink labels and URLs you define. Select one of the following from the list: Phases
, Process Cells
, Resources
, or Units.
The
Descriptors
area allows you to enter up to five hyperlink labels for each resource type. These labels are used within the resource’s Edit
dialog box.The
Default Values
area allows you to assign default URLs to each hyperlink label defined for the selected resource type. Enter the URL address for the hyperlink in the box that corresponds to the correct hyperlink label. The label in box 1
of the Descriptors
area corresponds to the URL address in box 1
of the Default Values
area. Default URLs can be overwritten when a specific resource type instance is edited.
TIP:
If a hyperlink value is not defined, either as a default or when the specific resource
type instance is created, the hyperlink label is not visible in .
e
ProcedureProvide Feedback