The FactoryTalk Batch Server
The
FactoryTalk Batch
Server is the FactoryTalk Batch
component that controls and coordinates system information, phases, and recipes. The FactoryTalk Batch
Server allows integration with process-connected devices and third-party software
packages. The FactoryTalk Batch
Server must be started and remain active during all batch functions.Provide Feedback