FactoryTalk Batch Server service configuration
FactoryTalk Batch
Server configuration can be verified and customized as needed. Configuration includes
specifying the startup method (Automatic or Manual), specifying the restart type (Warm, Warm
All, or Cold), and setting the server options.
TIP:
The
FactoryTalk Batch
Server service is configured to run as a Windows Server 2012 user. Changing the user
account in which the server runs is done through Services.Provide Feedback