Use automatic restart control to restart the FactoryTalk Batch Server
The
FactoryTalk Batch
Server maintains a detailed record of every recipe’s state as the recipe is running. If the server computer were to lose power or otherwise fail, use the automatic restart control feature to restart the server. Upon restarting the server on a failed server node, the following functions are placed into the state that existed prior to termination of the server:- Control Recipes
- Semi-Auto Phase Control
- Arbitration
Provide Feedback