Restart the FactoryTalk Batch Server

If the
FactoryTalk Batch
Server computer experiences a system failure, then restarting the computer starts the server. However, if the
FactoryTalk Batch
Server service fails, then you need to restart the service using the
FactoryTalk Batch
Service Manager.
To restart the FactoryTalk Batch Server
:
  1. Open
    FactoryTalk Batch
    . Batches on the batch list prior to the failure are still on the batch list. All batches that had phases in an active state now have transitions in the HELD state, and are in MANUAL mode with a failure.
  2. Select the batch, and then select
    Auto
    to place a batch in AUTOMATIC mode.
  3. Select
    Clear All Failures
    to clear the failures.
  4. Select the batch, and then select
    Restart Batch
    . The previously active phases return to a RUNNING state and the batch completes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal