Perform a manual failover

FactoryTalk Batch
can be configured to store batch journals and batch restart information in two separate locations. The use of a secondary server allows you to perform a manual failover if there is a hardware failure on the primary
FactoryTalk Batch
Server. The second computer must be capable of running the server.
You must install your area model file and all recipe files (and all instruction files if using
e
Procedure
) on both the primary server and the secondary server.
TIP:
Archiver recovery
- As part of the manual failover procedure you must manually copy the
eventdir.txt
and the
archque.txt
from the primary directory to the secondary directory.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal