Configure the FactoryTalk Batch Server for manual failover
When the
FactoryTalk Batch
Server fails, complete these steps.
TIP:
If you are using
FactoryTalk Batch
Material Manager
, refer to the procedure for material-enabled configuration.To configure the FactoryTalk Batch Server for manual failove
r:- Start the process-connected device communication software on the secondary server. The secondary server computer needs to communicate with the process controller that is running the phase logic.
- Ensure that the secondary server’s project directories are assigned to local directories in theServer Optionsdialog box located inFactoryTalk Batch Equipment Editor.
- Use theFactoryTalk BatchService Manager to start theFactoryTalk BatchServer on the secondary server computer, selectWarmorWarm Allas the startup type. The secondary server allows the batches to be restarted based upon information written by the primary server.
- (optional) If you are also using, use theeProcedureFactoryTalk BatchService Manager to start theServer on the secondary server computer.eProcedure
- For each computer runningFactoryTalk Batch View, enter the secondary server’s computer name as the NET registry key value.
- Stop and restart eachFactoryTalk Batch Viewinstance and any other software that communicates directly with theFactoryTalk BatchServer. This causes the instance to connect with the secondary server.TIP:The existing batches are placed in the MANUAL mode with transitions in the HELD state. Place the batches in AUTOMATIC mode, clear the failures, and then restart the batch.
Provide Feedback