Modify the .NET registry key
The .NET registry key contains the
FactoryTalk Batch
Server computer name and is used by remote clients to locate the server computer. During
a FactoryTalk Batch
Client computer installation, the setup program prompts you
for the server computer name and then places the name into the .NET key. In the event that
you change the server computer name, or if you are switching control to another FactoryTalk Batch
Server computer, you need to manually modify the .NET registry key on all remote client
computers to point to the server computer.To modify the .NET registry key
:- Open the Registry Editor.
- Select the HKEY_LOCAL_MACHINE on Local Machinewindow.Navigate to theSOFTWARE\BATCHCTL\Netsubkey.
- Double-click theServerregistry value.
- Modify the value data: Server = <MachineName>, where <MachineName> is the computer name on which theFactoryTalk BatchServer is installed.
Provide Feedback