Server Options dialog box - Batch Reporting tab
Use the
Batch Reporting
tab to select the reporting application for generating batch reports and archiving Batch data. Never
is the default reporting application.
Reporting Application | Description |
|---|---|
Report Editor | As of version 10.00, the Report Editor functionality is no longer supported or available. If you are currently using the Report Editor functionality, it is recommended that you transition to a different reporting solution. |
Archiver (End of Batch) | Defers control of batch reporting to FactoryTalk Event Archiver and only performs batch reporting upon removal of the batch from the Batch List. See instructions, Perform end of batch archiving. |
Archiver (Incremental) | Defers control of batch archiving to FactoryTalk Event Archiver and performs batch reporting at user-defined intervals during batch execution. See instructions, Perform incremental archiving |
User Defined (End of Batch) | Defers control of batch archiving to FactoryTalk Event Archiver and to perform batch reporting at user-defined intervals during batch execution. See instructions, Perform user-defined end of batch |
None (Queue Maintained) | Select this option if no batch reporting or archiving application is to be used. |
Never (No Queue) | Does not maintain a queue. This is the default selection. IMPORTANT: The Never setting causes the archiver queue file to not get written to. For a custom archiver and when writing to this queue file, use a setting other than Never and manually maintain the size of the archive queue file. |
Provide Feedback