Perform incremental archiving

Use
Archiver (Incremental)
to defer control of batch archiving to
FactoryTalk Event Archiver
and to perform batch reporting at user-defined intervals during batch execution. Specify the Incremental period between active archiving in
Minutes
or
Seconds
. The minimum setting is 5 seconds. The maximum is 9999 minutes. Setting the value outside of this range causes
FactoryTalk Event Archiver
to run in 5 minute incremental periods.
To update the incremental period after making changes, stop and restart the Incremental Archiver.
Configure the Incremental Archiver with a Windows user account that has administrative privileges to log on to the system. When using incremental archiving, configure
FactoryTalk Event Archiver
to run as a Windows service with an automatic startup type. Use the
FactoryTalk Batch
Service Manager to monitor and control
FactoryTalk Event Archiver
service. (See the
FactoryTalk Event Archiver
User Guide
for information on enabling
FactoryTalk Event Archiver
as a service.)
To perform incremental archiving
:
  1. Select
    Archiver (Incremental)
    .
  2. In the
    Archiver
    area, select
    Delete files after archive
    to enable the deletion of the
    .evt
    or .
    evtj
    files after
    FactoryTalk Event Archiver
    has stored the data in the ODBC database.
    IMPORTANT:
    Deleting files after archiving is not a reversible action and is not recommended.
  3. In
    Table Name
    , type the name of the table that contains the batch data. (The default is
    BATCHHIS
    .)
  4. In
    Incremental Period
    , type a value and select
    Minutes
    or
    Seconds
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal