Perform user-defined end of batch

Select
User-Defined (End of Batch)
to define a batch reporting application that is not listed in the Reporting Application area. Specify paths and names of the application’s .ini and .exe files.
To perform user-defined end of batch
:
  1. Select
    User-Defined (End of Batch)
    .
  2. Select the
    Executable File
    browse button to locate the application’s executable file. The dialog box opens.
  3. In the
    Select Archiver Executable File
    dialog box, select the appropriate .exe file, and then select
    Open
    .
  4. Select the
    Initialization File
    browse button to locate the application’s initialization file.
  5. In the
    Select Archiver Initialization File
    dialog box, select the appropriate .ini file, and then select
    Open
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal