Never
Does not maintain a queue. This is the default selection.
IMPORTANT:
The
Never
setting causes the archiver queue file to not get written to. For a custom archiver and when writing to this queue file, use a setting other than Never
and manually maintain the size of the archive queue file.Provide Feedback