Server Options dialog box - Project Settings tab

The default project settings for a computer on which the
FactoryTalk Batch
Server is installed are universal naming convention (UNC) names for all except the
Initialization File Name
. If the server is installed on another computer, then the
Initialization File Name
would use UNC names.
FTB_admin_ServerOpts_ProjectSettings
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal