Set project directories

Set directories for the following: Primary Journal, Secondary Journal, Error Logging, Instructions (if you are using
FactoryTalk
e
Procedure
), and Equipment Database.
IMPORTANT:
The
Primary Journal
path must be defined or the
FactoryTalk Batch
Server will not start. The
Primary Journal
path must be on the server computer in the BATCHCTL share. In addition, if the
Primary Journal
or
Secondary Journal
path is invalid, the server will not start. If an invalid path is used, an error message indicating the invalid path is written to the
batchsvr.log
file.
To set project directories
:
  1. In
    FactoryTalk Batch Equipment Editor
    , select
    Options > Server Options
    .
  2. Select the
    Project Settings
    tab.
  3. Select
    Browse
    to open the
    Select Directory
    dialog box.
  4. Select the appropriate directory, and then select
    OK
    to return to the
    Server Options
    dialog box. The selected UNC directory path name is inserted into the appropriate box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal