Recipe versioning

Below the
Store Recipes Using
area is the
Enable Recipe Versioning
check box. Check this box to enable Recipe Versioning, a system-enforced naming convention that stores and protects recipe revisions. By default the box is unchecked and recipe versioning is disabled.
IMPORTANT:
FactoryTalk
Full Edit access to
FactoryTalk Batch Equipment Editor
is required to enable and disable recipe versioning.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal