Material Policies tab

These features are used in conjunction with
FactoryTalk Batch
Material Manager
only.
  • Option When Material Server Communication is lost
  • Hold on Split Feed
FTBMM_Admin_server_options_material_policies_3_B12
Option when Material Server Communication is lost
When communication with the Material server is lost, these two options are available:
Failure and Hold
or
Switch to Manual
.
By default, the
FactoryTalk Batch
Server is configured to
Failure and Hold
. In this case, batches are placed in the HELD state when communication with the Material server is lost. The
FactoryTalk Batch
Server automatically resumes communication with the Material server when it becomes available.
To run batches even when communication is lost, configure the
FactoryTalk Batch
Server to
Switch to Manual
. In Manual mode, the server prompts the operator for information normally supplied by the Material Server. Restore the communication manually when the Material server becomes available. (For more information on restoring communication manually, see the
FactoryTalk Batch
Material Manager
Administrator Guide
.)
Hold on split feed
Select
Yes
to hold batches or
No
to continue to run batches in the event of a split feed.
The default is
Yes
and the batch is HELD when a split feed occurs.
When selecting
No
create a loop in the recipe so that the binding process can select another container for material additions when a split feed occurs. Add a material loop to the recipe with the
Create Material Loop
button in
FactoryTalk Batch Recipe Editor
. (For information regarding material loops, see the
FactoryTalk Batch Recipe Editor
User Guide
.)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal