Miscellaneous
The
Miscellaneous
area allows you to define options relating to the batchsvr.log and the batchSvr.ini file.The
Maximum Log File Size
box allows you to input the maximum size (in bytes) for the log file. When the log file reaches the maximum specified size, all new data is appended to the top of the log and old information is overwritten.The
Minimum Disk Space
box allows you to input the minimum disk space (in bytes) that must be available before a batch can be added to batch list. This helps to avoid data loss due to inadequate disk space.The
Default Batch ID
box allows you to specify a default batch ID; this batch ID automatically populates the Batch ID box when each batch is created.Enable Event Journals Signatures
turns event journal signatures on or off. The Event
Journal Signature function is a tool for detecting any unauthorized changes to electronic
batch records (.evt or .evtj files). (See the FactoryTalk Batch
System Files Reference Guide
TIP:
Do not edit the batchsvr.log or batchsvr.ini files directly unless you are specifically
instructed to do so by Rockwell Automation Technical Support. The
batchsvr.ini
file
contains data items that determine the configuration of the FactoryTalk Batch
Server and how the server operates in relation to the other FactoryTalk Batch
components.Provide Feedback