Send message to the operator and clearing message requests
The set of possible messages that may be sent by the phase logic is configured when the associated phase is defined in the area model using
FactoryTalk Batch Equipment Editor
. Each operator message is configured with a message ID, a positive integer. Requests to send a message refer to the message using the message ID. During batch execution, phase logic can make a request to the FactoryTalk Batch
Server to send a message to the FactoryTalk Batch View
and place the message into the electronic batch record.A
Send Message to Operator
request displays a message to the operator. In FactoryTalk Batch View
, it displays on the Phase Summary
screen. This type of request does not provide a mechanism to solicit information from the operator.The phase logic can also be configured to send a
Clear Message to Operator
request. This request clears the currently displayed message.Provide Feedback