Operation Sequence report

The Operation Sequence report displays the association and Operation Sequence data for
FactoryTalk Batch
and
SequenceManager
events. This report includes a header section and the Associated Operation Sequences and Associated Operation Sequences - Details tables. The header displays the specifics of the batch, such as:
Header name
For FactoryTalk Batch, displays
For SequenceManager, displays
Batch ID
Batch ID
Sequence ID
Unique ID
FactoryTalk Batch Unique ID
SequenceManager Unique ID
Recipe Name
Recipe Name
Sequence Name
Area Name
Area
Controller Serial Number
Process Cell
Process Cell
Controller Serial Number
Product Code
Product Code
Blank for SequenceManager
Product Description
Procedure Description
Extended Text
Completion State
—
—
Start Time
—
—
End Time
—
—
Duration
—
—
Event Archiver Operation Sequence Summary Report
For each associated Operation Sequence ID, select the Yellow Tag EA_BatchReportsYellowTag_icon to open the Batch Summary report. See the
Batch Summary report
for more information.
Associated Operation Sequences - Details
Event Archiver Operation Sequence Detail Report
  • The version of the FactoryTalk Batch report provides the following information:
    • When the report was last modified.
    • The version of the report that is currently installed.
    • If a custom report is based on a particular version of a report, it shows which version of the report was used.
This report has hyperlinks to these reports:
Icon
Destination Report
White Tag
Batch Listing
Yellow Tag
Batch Summary
White Arrow
Backward Tracing
Clock
Batch Execution
This report features filters for the following:
Filter name
Description
Start Time
Filters based on start time. Select NULL to filter from the beginning of collected time.
End Time
Filters based on end time. Select NULL to filter to the end of collected time.
Batch ID Filter
Accepts search criteria in the form of a
Batch Name
. Use the asterisk (*) as a wildcard character.
Process Cell
Filters based on the process cell name or controller serial number.
Recipe Name
Filters based on the recipe name or the sequence name.
Unit Name
Filters based on the unit name or the sequence unit ID.
Unique ID
Specifies which records display in the report.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal