FactoryTalk Event Archiver with Reporting Services

Create simple to advanced batch reports using
FactoryTalk Event Archiver
with Reporting Services along with
SQL Server
and
SQL Server
Reporting Services (SSRS).
FactoryTalk Event Archiver
with Reporting Services can:
  • Run the sample reports.
  • Create reports using the samples as templates for data source, report datasets, or layouts.
  • Create interactive and advanced custom batch reports that include selections, report detail drill-down, grouping, filtering, charts, and more, using the advanced sample reports.
Updates to the
BatchHistoryEx
database overwrite any customizations made to these reports.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal