Batch Execution report

The Batch Execution report displays an Execution Timeline of a batch. The Batch Execution report includes Operation Sequences from both
FactoryTalk Batch
and
SequenceManager
events. This report includes a header section and charts. The header displays the specifics of the batch, such as:
Header name
For FactoryTalk Batch, displays
For SequenceManager, displays
Batch ID
Batch ID
Sequence ID
Unique ID
FactoryTalk Batch Unique ID
SequenceManager Unique ID
Recipe Name
Recipe Name
Sequence Name
Area Name
Area
Controller Serial Number
Process Cell
Process Cell
Controller Serial Number
Product Code
Product Code
Blank for SequenceManager
Product Description
Procedure Description
Extended Text
Formulation Name
Recipe Formulation Name. If formulation parameters are not passed, or are an empty string, "Default Formulation" displays.
Blank for SequenceManager
Formulation Description
Recipe Formulation Description. If formulation parameters are not passed, or are an empty string, the description is empty.
Blank for SequenceManager
Completion State
—
—
Start Time
—
—
End Time
—
—
Duration
—
—
The charts are Unit Procedures, Operations, and Phases. Each displays the duration in seconds.
EA Batch Execution
  • The version of the FactoryTalk Batch report provides the following information:
    • When the report was last modified.
    • The version of the report that is currently installed.
    • If a custom report is based on a particular version of a report, it shows which version of the report was used.
There is a hyperlink to return to the Batch Listing report. This hyperlink does not pass any parameters back to the Batch Listing report.
This report features filters for the following:
Filter name
Description
Start Time
Filters based on start time. Select NULL to filter from the beginning of collected time.
End Time
Filters based on end time. Select NULL to filter to the end of collected time.
Batch ID Filter
Accepts search criteria in the form of a
Batch Name
. Use the asterisk (*) as a wildcard character.
Process Cell
Filters based on the process cell name or controller serial number.
Recipe Name
Filters based on the recipe name or the sequence name.
Unit Name
Filters based on the unit name or the sequence unit ID.
Unique ID
Specifies which records display in the report.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal