Event Summary report

The Event Summary report displays a custom event summary based on report parameter filter selection. The report displays event records from one event journal based on the Unique ID specified. This report includes a header section and an Event Record Data table. The header displays the specifics of the batch:
Event Summary Header
The header includes:
Header name
For
FactoryTalk Batch
, displays
For
SequenceManager
, displays
Event file name
—
—
Batch ID
Batch ID
Sequence ID
Unique ID
FactoryTalk Batch
Unique ID
SequenceManager
Unique ID
Recipe Name
Recipe Name
Sequence Name
Area Name
Area
Controller Serial Number
Process Cell
Process Cell
Controller Serial Number
Product Code
Product Code
Blank for
SequenceManager
Product Description
Procedure Description
Extended Text
Report Status
—
—
Report Generated By
—
—
Report Time
—
—
Row Count
—
—
Columns in the Event Record Data table can be sorted in ascending or descending order.
EA Event Summary Report
  • The version of the FactoryTalk Batch report provides the following information:
    • When the report was last modified.
    • The version of the report that is currently installed.
    • If a custom report is based on a particular version of a report, it shows which version of the report was used.
This report features filters for the following:
Filter name
Description
Start Time
Filters based on start time. Select NULL to filter from the beginning of collected time.
End Time
Filters based on end time. Select NULL to filter to the end of collected time.
Batch ID Filter
Accepts search criteria in the form of a
Batch Name
. Use the asterisk (*) as a wildcard character.
Process Cell
Filters based on the process cell name or controller serial number.
Recipe Name
Filters based on the recipe name or the sequence name.
Unit Name
Filters based on the
FactoryTalk Batch
unit name or unit ID; or the sequence unit ID.
Unique ID
Specifies which event records display in the report.
Event
Specifies which event records to include or exclude in the report based on event type.
Description
Specifies which event records to include or exclude in the report based on the event description.
Value
Specifies which event records to include or exclude in the report based on event value, such as recipe header information, scale factor, recipe value change, system message, state change, and so on.
Columns
Specifies which columns to display in the report.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal