PC-based phase properties
To enable communication between a PC-based phase and the
FactoryTalk Batch
Server, properties can be modified in two ways:- With the phase selected, use thePropertieswindow to locate and set the appropriate properties, or
- Use the customProperty Pagesdialog box.
All properties specific to the
Batch Phase Execution
control that can be configured at design time are included in this dialog box. Provide Feedback