Set custom properties in the Property Pages dialog box
Use the
Property Pages
dialog box to set custom properties to enable communication between a PC-based phase and the FactoryTalk Batch
Server.
IMPORTANT:
If you attempt to configure a property at design time with an invalid entry, you are notified of the error by a message box, which includes a range of valid entries.
If you attempt to configure a property at design time that does not support configuration at design time, a message box opens.
If you attempt to configure a property at runtime that does not support modification at runtime, an entry is written to the activity log file.
To set custom properties in the Property Pages dialog box
:- Right-click theBatch Phase Executioncontrol and selectProperties. TheProperty Pagesdialog box opens with theConfigurationtab selected.

- Enter the values for the custom configuration properties.
- SelectApply.
- Select theOperationtab and enter the values for the custom operation properties.

- SelectApply, thenOK.
Provide Feedback