ProcessCellIDUnits
The
ProcessCellIDUnits
item returns information about all units in a process cell, including how they are linked.This table shows the input and output formats for this item.
Input Format | Request only: ProcessCellIDUnits While Advise will return information, it would not normally be used as the data does not change during processing. | ||
ProcessCellID | is | ASCII – Integer, the unique Equipment ID corresponding to the process cell | |
Output Format | The ProcessCellIDUnits item returns in this format: | ||
<PCellIDUnits> | is | <NullList> | <UnitList> | |
<NullList> | is | CString.Empty() \crlf | |
<UnitList> | is | <UnitData> \crlf | <UnitData> \crlf <UnitList> | |
<UnitData> | is | <UnitID> \t <UnitName> \t <UnitClass> \t <MaxOwners> \t <XCord> \t <YCord> \t <BitMapIndex> \t <Connections> | |
where <UnitData> is: | |||
Field Name | Format | Description | |
<UnitID> | ASCII - Integer | Resource ID configured in FactoryTalk Batch Equipment Editor . | |
<UnitName> | ASCII - String | Unit Name. | |
<UnitClass> | ASCII - String | Unit Class Name. | |
<MaxOwners> | ASCII - Integer | Max # of Owners as configured in FactoryTalk Batch Equipment Editor . | |
<XCord> | ASCII - Integer | X Coordinate for Equipment View. | |
<YCord> | ASCII - Integer | Y Coordinate for Equipment View. | |
<BitMapIndex> | ASCII - Integer | Location of bitmap in the list of Unit Bitmaps item. | |
<Connections> | Variable | Information about the units to which this unit is connected. | |
where <Connections> is: | |||
<Connections> | is | $CONN \t <ConnData> \t $END | |
<ConnData> | is | <NullConnList> | <ConnList> | |
<NullConnList> | is | \t \t | |
<ConnList> | is | <UnitName> \t <UnitID> | |
where <ConnList> is: | |||
Field Name | Format | Description | |
<UnitName> | ASCII - String | Unit Name. | |
<UnitID> | ASCII - Integer | Resource ID configured in FactoryTalk Batch Equipment Editor . | |
This table shows an example of the return on this request.
Example: | A request on object . GetItem(54Units) could return:55 \t NP_MIXER1 \t MBR_MIXER_CLS \t 1 \t 194 \t 54 \t 8 \t $CONN \t NP_FREEZER1 \t 67 \t $END \crlf 84 \t NP_MIXER2 \t MBR_MIXER_CLS \t 1 \t 392 \t 54 \t 9 \t $CONN \t NP_FREEZER2 \t 85 \t $END \crlf 85 \t NP_FREEZER2 \t MBR_FREEZER_CLS \t 1 \t 392 \t 242 \t 11 \t $CONN \t \t $END \crlf 67 \t NP_FREEZER1 \t MBR_FREEZER_CLS \t 1 \t 194 \t 246 \t 10 \t $CONN \t \t $END \crlf |
Provide Feedback