View audit messages in the FactoryTalk AssetCentre client
View the audit messages through the
FactoryTalk
AssetCentre client. To view the audit messages in the FactoryTalk AssetCentre client
:- To open theFactoryTalkAssetCentre client,Startbutton, point toAll Programs > Rockwell Software >, and then clickFactoryTalkAssetCentreFactoryTalkAssetCentre.
- Click theLogsbutton to open the Logs view.Tip:For information about using or customizing theFactoryTalkAssetCentre client, refer to the utility's online help or the.FactoryTalkAssetCentre Installation Guide
Provide Feedback