FactoryTalk AssetCentre Client

When
FactoryTalk AssetCentre
is installed, and auditing is enabled for
FactoryTalk Batch Equipment Editor
and
FactoryTalk Batch Recipe Editor
, view the audit messages through the
FactoryTalk AssetCentre
Client.
TIP:
To use
FactoryTalk AssetCentre
for auditing, Change Management (
FactoryTalk AssetCentre
add-on solution) must be installed.
The graphic illustrates an audit log as viewed with the
FactoryTalk AssetCentre
Client. The
FactoryTalk Batch
audit messages are written to the
Message Summary
field. Only the first 100 characters of the
Message Summary
field are displayed on a line. The entire message is displayed in the Details window. The
EditedObject
audit message field is used to populate the
Resource
field in the Viewer.
FTB_FTAssetCentre Audit View_B12
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal