Audit messages
When auditing is enabled for
FactoryTalk Batch Equipment Editor
and FactoryTalk Batch Recipe Editor
, view the audit messages through the Diagnostics Viewer or the FactoryTalk AssetCentre
client.
TIP:
Batch audit messages are generated in two formats: Engineer Audit and Secure Audit. The
audit messages formatted for the local log are categorized as Engineer, and audit messages
formatted for
FactoryTalk AssetCentre
are categorized as Secure. If FactoryTalk AssetCentre
is installed, a Secured logging destination is enabled and messages can be routed to
both the local and FactoryTalk AssetCentre
log.Provide Feedback