FactoryTalk Batch audit trail
FactoryTalk Batch
auditing provides a detailed audit trail of user-initiated changes from FactoryTalk Batch Equipment Editor
and FactoryTalk Batch Recipe Editor
.FactoryTalk Batch Equipment Editor
and FactoryTalk Batch Recipe Editor
track all changes in the current editing session for each user-initiated action. When
changes are saved, each entry in the list generates an audit message. If changes are made,
but are not saved, no audit message is generated.Audit messages are forwarded from the
FactoryTalk Batch Equipment Editor
and FactoryTalk Batch Recipe Editor
to FactoryTalk
Diagnostics, a Rockwell Software product that enables application logging and auditing,
or to FactoryTalk AssetCentre
(if installed).
TIP:
Batch audit messages are generated in two formats: Engineer Audit and Secure Audit. The
audit messages formatted for the local log are categorized as Engineer, and audit messages
formatted for
FactoryTalk AssetCentre
are categorized as Secure. If FactoryTalk AssetCentre
is installed, a Secured logging destination is enabled and messages can be routed to
both the local and FactoryTalk AssetCentre
log.The
FactoryTalk Directory
System
folder contains Audit settings that apply to all FactoryTalk
-enabled products in a system. The FactoryTalk
Audit Policy Setting, Audit changes to configuration and control system
, must be
enabled to display audit messages in either the FactoryTalk
Diagnostics Viewer or the FactoryTalk AssetCentre
client. This FactoryTalk
policy setting overrides the registry settings used to enable and disable auditing in FactoryTalk Batch Equipment Editor
and FactoryTalk Batch Recipe Editor
. (For more information see FactoryTalk
Help, located in the FactoryTalk Administration Console
.)Provide Feedback