Audited FactoryTalk Batch Recipe Editor events
This section describes the set of audit messages generated by
FactoryTalk Batch Recipe Editor
in response to recipe modifications and operations.Message Type | Event |
|---|---|
Recipe Object | Open an existing recipe Create a new recipe Save a recipe, including master recipes and recipe formulations Save all recipes, including master recipes and recipe formulations Remove a recipe (User-supplied comment when deleting) Import a recipe (User-supplied comment when importing) Export a recipe (User-supplied comment when exporting) Rebuild the recipe directory (User-supplied comment when rebuilding recipe) Delete an existing recipe, including master recipes and recipe formulations Update an existing recipe, including master recipes and recipe formulations |
Recipe Print | Print a procedure, unit procedure, or operation |
Recipe Header | Edit/update recipe header properties, except the recipe name |
Recipe Step | Add a recipe step, insert step, or parallel recipe step Edit/update a recipe step Delete a recipe step |
Recipe Approval Step | Signoff on an approval step Revert an approval step |
Recipe Versioning | Check in a recipe (create a new version of a recipe) Check out a recipe (create a work-in-progress (WIP) recipe) Obsolete a recipe Save an obsolete recipe Reinstate an obsolete recipe Save a reinstated recipe Version conflict on recipe import Version conflict on recipe directory rebuild, including auto-rebuild of the
directory when FactoryTalk Batch Recipe Editor opensDelete a recipe due to version conflict resolution during import or recipe directory rebuild Remove signoff(s) due to verification failure for versioned and non-versioned recipes |
Recipe Security | Change a recipe security state Edit/modify a security authority identifier (SAI) Change a FactoryTalk Services Platform SAI host computer |
Recipe Text Box | Add a text box Delete a text box Edit a text box (only if the comment changes) Associate a text box Disassociate a text box |
Recipe Formula Parameter | Add a recipe formula parameter to a step Delete a recipe formula parameter from a step Edit/update a recipe formula parameter of a step |
Recipe Formulation | Add a recipe formulation Delete a recipe formulation Rename a recipe formulation Change the recipe formulation description |
Recipe Formulation Parameter | Edit/update a recipe formulation parameter |
Formula Value | Edit/update a formula value’s non-origin properties Edit/update a formula value’s origin property Edit/update a formula value’s value property for deferred parameters |
Report Limit | Add a report limit Delete a report limit Edit/update a report limit |
Bind Requirement | Add/update a bind requirement Delete a bind requirement |
Bind Preference | Add/update bind preference Delete a bind preference |
Recipe Transition | Add a transition to a recipe Edit/update a recipe transition Delete a transition to a recipe |
Link Group | Add a recipe link group Delete a recipe link group Edit/update a recipe link group |
Equipment Requirement | Add an equipment requirement to a recipe Delete an equipment requirement of a recipe Edit/update procedure-only equipment requirement properties, except downstream units Edit/update procedure-only equipment requirement’s downstream units property Edit/update operation and unit procedure equipment requirements |
Recipe Verification | Verify a single recipe Verify all recipes |
Material Loop | Add a material loop to a recipe Undo a material loop |
Recipe Link | Add a recipe link Delete a recipe link |
Provide Feedback