Enable auditing for FactoryTalk Equipment Editor or FactoryTalk Recipe Editor

Use the
FactoryTalk Administration Console
to modify the policy settings for auditing. These policy settings are located in both the
FactoryTalk
Network Directory and Local Directory. The Local Directory audit policy overrides the Network Directory audit policies.
TIP:
The
FactoryTalk
Audit Policy Setting,
Audit changes to configuration and control system
, must be enabled to display audit messages in
FactoryTalk
Diagnostics or
FactoryTalk AssetCentre
.
To enable auditing for
FactoryTalk Batch Equipment Editor
or
FactoryTalk Batch Equipment Editor
:
  1. Open the
    FactoryTalk Administration Console
    and log on to the Network Directory or Local Directory.
  2. Navigate to
    System > Policies > System Policies
    .
  3. Right-click
    Audit Policy
    , and select
    Properties
    .
  4. Select
    Audit changes to configuration and control system
    and set it to
    Enabled
    . Auditing is enabled the next time
    FactoryTalk Batch Equipment Editor
    or
    FactoryTalk Batch Recipe Editor
    runs.
    TIP:
    Restart all
    FactoryTalk Batch
    components to update changes made in the
    FactoryTalk Diagnostics
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal