Viewer message fields
The audit messages for
FactoryTalk AssetCentre
are formatted as closely as possible as those used in FactoryTalk
Diagnostics Viewer messages. The Resource
field for audit messages contains the
value of the Edited Object
field of a diagnostics message.The
Message
field contains these fields:- User comment
- Action
- Area
- ContainingObject
- ContainingObjectID
- EditedObject
- EditedObjectID
- EditedProperty
- EquipmentPhase
- NewValue
- OldValue
- Operation
- Procedure
- ProcessCell
- SubAction
- SubObject
- SubObjectID
- Unit
- UnitProcedure
- WorkingSet
Each entry consists of a Label and its associated data. Each entry also contains tab characters to line up the data for readability, and is followed by a new line character.
Provide Feedback