Command
The
COMMAND
execute commands a procedure to a desired state or mode.The format and return for this execute includes:
Execute Format | A FactoryTalk Batch Server supports an execute with this format:[COMMAND( Item,UserID,ProcedureID,Cmd )] | ||
where: | Item | Item name as specified by the client. | |
UserID | User identification entered into the event journal associated with this event. | ||
ProcedureID | Unique hierarchical path name to the procedure, unit procedure, operation or phase: Procedure: CreateID Unit Procedure: CreateID \t UnitProcIDName Operation: CreateID \t UnitProcIDName \t OperIDName Phase: CreateID \t UnitProcIDName \t OperIDName \t PhaseIDName | ||
Cmd | Command either to change the state or mode. Commands which may be issued are:
The command must be valid for the procedure level being commanded. | ||
where: | <FullPath> | is | <CreateID> | <CreateID> /t <Path> |
<Path> | is | <StepIdentifier> | <StepIdentifier> /t <Path> | |
where: | |||
Field | Format | Description | |
<CreateID> | ASCII - Integer | Unique batch ID assigned by the FactoryTalk Batch Server. | |
<StepIdentifier> | ASCII – String | Step identifier (for example, Mix:1) | |
Action | A successful COMMAND execute results in either the command being issued to the specified procedure element, or in the command being queued pending completion of the confirmation signature. A COMMAND execute results in a failure message when the Command sent is equal to the current batch state. Example: If a batch is running and a START or RESTART execute is issued, the command will return a failure message. | ||
Return Format | The item populates with this data: SUCCESS: | SUCCESS: <ActionID> | FAIL: <message> | ||
where: | |||
Field | Format | Description | |
<ActionID> | ASCII – Integer | Action ID associated with the signature(s) generated in response to the execute. | |
<message> | ASCII - String | Error message appropriately formatted for operator display. | |
The following table shows an example of the return on this execute.
Example: | An execute string consisting of: COMMAND(Item,Station2/View,36,START) Could return: SUCCESS:997 |
Provide Feedback