ResourceIDStrings
The
ResourceIDStrings
item returns the list of five generic strings associated with the identified resource.This table shows the input and output formats for this item.
Input Format | Request: ResourceIDStrings | ||
ResourceID | is | ASCII - String, the | |
Output Format | The ResourceIDStrings item returns in this format: <ResourceName> \t <GenericString1> \t <GenericString2> \t <GenericString3> \t <enericString4> \t <GenericString5> | ||
where: | |||
Field Name | Format | Description | |
<ResourceName> | ASCII - String | Name of the resource. | |
This table shows an example of the return on this request.
Example: | A request on object . GetItem(68Strings) could return:NP_ADDDAIRY_M1 \t CROSS INVOCATION LABEL 1 \t CROSS INVOCATION LABEL 2 \t CROSS INVOCATION LABEL 3 \t CROSS INVOCATION LABEL 4 \t CROSS INVOCATION LABEL 5 |
Provide Feedback