Command and arbitration masks
Command and arbitration masks are used as flags to represent available
FactoryTalk Batch
commands. Commands that cause recipes or phases to change states are included in the Command Masks
table. Commands that affect ownership of resources are included in the Arbitration Masks
table.Provide Feedback