Command masks
This table includes the individual commands used within the
Command Masks
table and their numeric values. The mask value in the Command Masks
table is the sum of each of the commands’ decimal values.Command | Decimal |
|---|---|
RESTART | 256 |
STOP | 4 |
ABORT | 1 |
COMMAND MASK | 261 |
Provide Feedback