PC-based phases
A PC-based phase allows you to program a phase outside of a process-connected device (PCD). You can program the phase to meet your own unique requirements from within your Microsoft-compatible control container. The PC-based phase works the same way as any phase defined in a PCD, communicating with the
FactoryTalk Batch
Server through the Batch Phase Execution
control. This saves your system’s memory for processes requiring interaction with hardware.After a PC-based phase is created, the
FactoryTalk Batch
area model must be updated to include the new phase and the appropriate equipment modules. Because the Batch Phase Execution
control behaves as a data server, a new data server definition must be created. The data server definition is created using FactoryTalk Batch Equipment Editor
, and defined using the Batch Phase Execution
control’s communication parameters. The phase can then be added to your recipes. The PC-based phase must remain active during recipe execution, allowing the phase to communicate with the FactoryTalk Batch
Server through the Batch Phase Execution
control.An activity log file is created for each PC-based phase when it runs. This log file,
Singleton.log
, is written to the WINDOWS\system32
directory.Provide Feedback