Create a PC-based phase

A PC-based phase is created using the
Batch Phase Execution
control and an OPC container application. The control is added to the container application, placed in the appropriate medium (form, spreadsheet, document, and so on), and its properties, methods, and events defined.
The instructions included in this section relate to creating a PC-based phase within
Visual Basic
. If you choose to implement a PC-based phase in an application other than
Visual Basic
, on the Control Toolbox, click
More Controls
to retrieve the
Batch Phase Execution
control.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal