Distribute PC-based phase applications

Please read the license agreement that was shipped with this software. You are bound by the licensing restrictions contained in the agreement. You can use all of the files accompanying this product for development use and redistribute the runtime version of the software in accordance with the terms of the license agreement.
TIP:
The
FactoryTalk Batch
Server is required for the
Batch Phase Execution
control to function and must be installed on the remote computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal