Parameter and report parameter limits

The
Batch Phase Execution
control can be configured to obtain the
Parameter
and
Report Parameter Limits
defined on a PC-based phase in the area model.
The PC-based phase, like any other phase, can be assigned a
Verification
method and associated with verification policies in the area model. Adding additional phase parameter tags and code to the
Batch Phase Execution
control application allows the parameter values to be downloaded for use in the control. Assigning verification policies to a PC-based phase can generate signature requests when parameter or report parameter limit values are too high or too low
.
If a PC-based phase has tag locking enabled, and limit tags enabled on the equipment module, additional limit tags are created. For example, if the phase parameter has a
Verification
method equal to
High/Low
, three additional tags are created for the equipment module as shown here:
  • Phasename
    .P01
    M
    - tag for the
    Verification
    method
  • Phasename
    .P01
    H -
    tag for the High Limit
  • Phasename
    .P01
    L -
    tag for the Low Limit
    TIP:
    Parameter limit tags and Report limit tags are created with a tag delimiter that must be removed when used with a PC-based phase.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal