Use a PC-based phase
After creating the PC-based phase executable, you must perform the following tasks:
- Update the area model inFactoryTalk Batch Equipment Editor
- Add the phase to your recipes usingFactoryTalk Batch Recipe Editor
The following table indicates the relationship between the PC-based phase property and the area model. You must adhere to the rules shown here to allow for proper communication.
PC-based phase property | Area model |
|---|---|
The OPC’s Watchdog Item Access Path | PC-based phase’s OPC Access Path for Tags , as defined in Visual Basic , or other container, or the Topic property (changing one also changes the other) |
PC-based phase Name property, as defined in Visual Basic , or other container | Equipment Module’s Tag name, as defined in FactoryTalk Batch Equipment Editor |
Provide Feedback