Add the new phase to a recipe

Use
FactoryTalk Batch Recipe Editor
to add the new phase to a recipe.
To add the new phase to a recipe
:
  1. Open
    FactoryTalk Batch Recipe Editor
    .
  2. Open the recipe where you want to add the new phase.
  3. Add the phase and associated transition to the recipe.
  4. Verify and save the recipe.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal