Run a recipe with a PC-based phase

The PC-based phase executable must be active when the recipe is processed.
To run a recipe with a PC-based phase
:
  1. Start the PC-based phase executable.
  2. Start the
    FactoryTalk Batch
    Server.
  3. Open the
    FactoryTalk Batch
    View or HMI application.
  4. Create a batch from the recipe containing the PC-based phase.
  5. Run the batch. The recipe phase interacts with the PC-based phase and performs its pre-programmed functions.
    The icon that represents the phase changes color based on the state of the phase. These color changes match the colors used in the
    FactoryTalk Batch
    View.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal