PC-based phase properties, methods, and events
A PC-based phase is created using the
Batch Phase Execution
control and an OPC container application. The control must be added to the container application, placed in the appropriate medium (form, spreadsheet, document, and so on), and its properties, methods, and events defined. This section defines those properties, methods and events.Provide Feedback