Phase Logic Requests
Use a Phase Logic Request to generate a signature request for a PC-based phase.
Before you can successfully use the General Signature Request, electronic signatures must be configured in the area model. Signature templates define the signature signoff information required to complete a signature request generated against a phase. Each signature can require up to three signoffs, which consist of security permissions and optional comments.
Provide Feedback