Add the control to the project
Use MFC to add the control to the project.
To add the control to the project
:- In MFC, selectProject>Add to Project.
- Select theComponents and Controlsoption.
- Open theRegistered ActiveX Controlsfolder.
- Select theBatch Phase Executioncontrol.
Provide Feedback