BLFailure_x
The batch in the batch list. This is the highest priority failure message for the steps running within the recipe.
BLFailure_x
item returns the failure message for the x
thThis table shows the input and output formats for this item.
Input Format | Request: BLFailure_ <RowNumber> | ||
<RowNumber> | is | ASCII - Integer An array index. When an unacknowledged prompt generates, it adds to an array. If the unacknowledged prompts list is not sorted, then x is the row number of the unacknowledged prompt appearing in the unacknowledged prompts list. | |
Output Format | The BLFailure_x item returns in this format: <Failure> | ||
Field Name | Format | Description | |
<Failure> | ASCII – String | Failure message for the batch appearing on x th | |
This table is an example of a typical batch list containing three batches with batch IDs BATCH_98, BATCH_99, and BATCH_100:
Batch ID | Recipe | Desc | Start Time | State | Failure |
BATCH_98 | Vanilla | Ice Cream 1 | 2/24/2022 1:22:02 pm | RUNNING | |
BATCH_99 | Chocolate | Ice Cream 2 | 2/24/2022 1:24:12 pm | RUNNING | |
BATCH_100 | Premium French Vanilla | Ice Cream 3 | 2/24/2022 1:32:30 pm | RUNNING | PHASE UNDER EXTERNAL CONTROL DETECTED |
This table shows an example of the return on this request.
TIP:
A request on
object.GetItem(BLFailure_3)
would return the failure field of the batch in the batch list’s third row:PHASE UNDER EXTERNAL CONTROL DETECTED
Provide Feedback